Other Parts Discussed in Thread: LMP8646, LM5176
Hi team
My customer has been using TL1451A. I received a question about current limiting of this device.
Customer is currently using at Vin=32V, Vout=28V.
1-1. Is it possible to set a current limit for this device? For example, when the output current reaches 5A, the current is limited, and if the limitation continues for more than 100ms, the device stops.
1-2. Could you provide the recommended circuit of the current limit?
2. Could you introduce a DC/DC converter which can meet following condition?
- Input voltage rating is 40V
-Output current 15A
-Vout accuracy is +/-1%
-Current limit function
-100% duty cycle
Regards,
Yamaguchi