This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL1451A: Current limit

Part Number: TL1451A
Other Parts Discussed in Thread: LMP8646, LM5176

Hi team

My customer has been using TL1451A. I received a question about current limiting of this device.

Customer is currently using at Vin=32V, Vout=28V.

1-1. Is it possible to set a current limit for this device? For example, when the output current reaches 5A, the current is limited, and if the limitation continues for more than 100ms, the device stops.

1-2. Could you provide the recommended circuit of the current limit?

2. Could you introduce a DC/DC converter which can meet following condition?

- Input voltage rating is 40V

-Output current 15A

-Vout accuracy is +/-1%

-Current limit function

-100% duty cycle

Regards,

Yamaguchi