I'm building a 16x16 LED matrix. According to the spec. description and the sample code, send First Line data, then input 65535 GCLK and the 2nd line data, repeat it 15 times. Then repeat the input of data and GCLK in a loop.
The color data of line 1 is blue to green gradients, the color data of line 2 is green to red gradients, same as line 3, line 4 etc.
But the actual color it shows is line 1-blue to green gradients with slightly red, line 2-seems to be just yellow. It seems to be the next line's color had combined with the currentline.According to the sample code, during the change of different line, the GPIO of different line has been compeletly shut down, and the digital multimeter shows they have been correctly shut down during the switch.
How could this happen, and how can i do to avoid this situation?