This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1825A-SP: 50% maximum duty cycle?

Part Number: UC1825A-SP
Other Parts Discussed in Thread: UC1825-SP, UC1825B-SP

The datasheet of UC1825A-SP said that “The UC1825A-SP outputs are alternately controlled”, so that duty cycle varies “from 0 to less than 50%”. However, in Fig. 15 of the datasheet, the maximum duty cycle can reach 100%. Besides, the datasheet of UC1825-SP does not have the description about the 50% limit of duty cycle. So, could you clarify: (1) what is the maximum output duty cycle of UC1825A-SP? (2) what is the maximum output duty cycle of UC1825-SP?