Team,
I have a customer who is using the TPS63050RMWR and then are measuring a 1.35Mhz switching frequency. The device is is regulating well, but it is not switching at the expected 2.5 Mhz... They are seeing poor EMI performance at 1.35 Mhz. The PFM pin is pulled high and is measuring 5V. The load current is about 300mA. When the load is increased to 400mA the frequency decreases to 900khz. Schematic follows webench and datasheet recommendations and nothing stood out to me. Any ideas on how this device could be switching at anything other than 2.5 Mhz?
Thank you!