Other Parts Discussed in Thread: UCD90160A
Hi ,
In my design the ennable pin of TPS54A20 is driven from a GPIO of another power device as below:
TPS54A20 ennable is driven from a device that can start after the 12V power supply of TPS54A20 is established. Because of this TPS54A20 ennable pin is floating and the TPS54A20 can start before the driving device is in function.
Would the below workaround with a pull down on the ennable pin will be OK as it is supposed to block the start of the TPS54A20 until the UCD90160A apply a 0 to 1 transition?
Is there any specific I should take care with such implementation?
Thanks