This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21320-Q1: UCC21320-Q1 Motor Driving Capabilities

Part Number: UCC21320-Q1

Hello,

I am planning to use UCC21320-Q1 to drive 4 pole BLDC Motors.

I would like to know can Channel A source current to the coil when turned on then sink away the current when turned off ? or do I need to use both channel A and B with the outputs tied together and have high and low sides operating independently for each coil ?

 

Also please share if you have any reference motor driving circuit.

 

Thanks,

Arif