Hello,
when I set the mode pin to ground, the output is 5.1V when I use FPWM it's only 4.65 Volt.
Why the voltage drop in FPWM mode?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
That's quite strange. Is it a constant 500mA load current or pulse load current?
What's the function of U10 HT7027? Could you supplies TPS61022 EN pin with a fixed logic high signal to make sure TPS61022 is always enabled? From your waveform in FPWM mode, it looks like when TPS61022 is enabled and switching, Vin drops so EN pin is pulled low. Then Vout decreases.
Hi,
I removed U10 and connect EN pin to VBAT directly, no change.
We turn on VIN by P-Channel MOSFET.
For further tests we fixed GATE to ground.
On SOURCE the voltage looks fine but on DRAIN VIN drops down.
This only happens in FPWM mode.
We use the same circuit with other Step-Up converters without any problems.
Hi ,
I think we should figure out why the input voltage has so much voltage drop.
It looks like when TPS61022 starts switching, TPS61022 draws a lot of current from battery through the PFET, the PFET has high voltage drop so Vin decreases, then device draws even more current until it shows down. Because TPS61022 is a higher current capability device, valley switch current limit is up to 7A, so PFET voltage drop is higher. I see the PFET current capability is 4A. It may have problem when TPS61022 output power is high.
To verify this, 1. Could you try remove or short the PFET drain to Source? Probe the inductor current or input current with current probe? 2. Use an external power supply which has enough current limit (>6A) to make sure the input voltage is stable.
Can you answer the question: That's quite strange. Is it a constant 500mA load current or pulse load current?