Hi Team,
I would like to get your input below regarding our customer inquiry with LM5175.
Design input 12V - 28V, output 14.6v 10A
The actual input voltage is 12V; the output voltage is 4.0V. Pin23 VCC has 6.8v, and VCC has 150Hz low pulse signal. Is the chip starting protection? What is the reason that the output voltage can not reach the design value?
BEST REGARDS
HU
Let me know if you have any questions with the customer.