I used web-bench to generate a LM5023 based design for an AC/DC power supply;
Vin 24 - 250Vac, Vout =12Vdc @1.5A
A number of custom components are specified. Web Bench does not support simulation for the resulting design. Is it safe to assume that for these specific resistors and cap that a value close to the ideal specified will not significantly degrade the performance and regulation?
- Rsnub1/2 = 5.9462kΩ (use with 5.94K 1%
- Rvin = 1.83967 kΩ (use 1.84kΩ ?)
- Cd = 5.5076pF
Assuming that I can select commercial diodes that meet stated specs, is there any other spec constraints I should be wary off?
- Dsec/Dsec2: VRRM 319, Io 3.75
- D3 VRRM 347V, Io 40mA
thanks