Hi team,
Should I disconnect D1 from the EVM to observe over voltage clamp operation shown in "Figure 3-1. LM74800EVM-CD Schematic" in its user's guide?
I found that LM74800EVM-CD can observe over voltage clamping operation by connecting 1-2 on J6 shown in "2.3 Over Voltage Protection (J6)" in its user's guide.
However I also found that D1 or 33V TVS diode is connected to input side and OV clamp voltage looks 37.5V rising and 34.5V falling.
Regards,
Ochi