Hi Team,
I would like to use TPS92314 at the conditions.
I have three questions.
<Our Conditions>
Input : 85VAC to 230VAC
Output: 5VDC / 1A(max)
Power factor: 0.7 to 0.9
------
[Q1]
I understand that TPS92314 is device for LED drive (constant current).
Can I use TPS92314 for the constant voltage?
------
[Q2]
I found “TPS92314_TPS92314A_Calculation_tools__REV1.1_version”.
However, I can’t set “output voltage=5V.
Because, I can’t select suitable “Number of LED in series” and “Normal LED forward voltage”.
Could you please let us know other calculation tools if you have any tools?
------
[Q3]
I would like to know the power factor at all output current conditions.
Do you have the calculation tools of power factor?
------
Regards,
Hide