Other Parts Discussed in Thread: LM5164
Hi TI Team,
For LM5164, we were analysing a failure mode if Vout (voltage after Cout) shorts to input voltage. We have observed that the FB pin voltage is rated only for 5.5V which can damage the IC.
Our current configuration is as follows:-
Vin Max = 70V, RFB1 = 440K, RFB2 = 49.9K Vout = 12V. As per calculations voltage at FB pin shall be 70*49.9/(49.9+440) = 8V
What protection scheme do you recommend to avoid this?
Thanks,
Rohan