Created a design via Webench, (18-60Vin / 12V@0.4A out) however actual build can only maintain 12V up to around 12mA after which it drops fairly precipitously, ie: 470ohm load drops to 3V. The layout is pretty close to what is recommended in the datasheet. I have tried increasing output C, tried a different diode, doubled Cboot to no effect. The switch waveform has a fair amount of ringing. I can provide all the documentation. Also, this is the Y versions of the LV2862.