This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28070A: Power limitation at high line

Part Number: UCC28070A
Other Parts Discussed in Thread: UCC28070, UCC28070EVM

Dear all,

 

Developing a 600W PFC with UCC28070 and searching into the TI forum without any success… (except Mark Walters 4 years ago, without any conclusion)

It seems to have a power limitation in high line. All parameters seems to be OK in Design tool, but I see Vrmo always at 3V and Vao near 4.6V @110Vac and 5V @230Vac. Irmo would change from 3V to 1V.

I have a doubt on C14 and C16 value.

 

I send you schematics, design tool and scope capture.

 

The scope legend is :

Yellow : C13 voltage

Pink : Vrmo (pikes ?)

Blue : Vcao

@110Vac Pout 400W => 438

@230Vac Pout 400W => 439

Thanks a lot,

  

 Design Tool.pdf