This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS752-Q1: GND/Heatsink Pin Connection

Part Number: TPS752-Q1

Hi Team,

Seeking your assistance in verifying if the pins  1, 10, 11 and 20 of the TPS752-Q1 (PWP package ) are indeed internally connected. Asking this as one of our customer has reported that they have performed continuity tests on multiple TPS75201QPWPRQ1 ICs but found that there are no connections between these pins. The pins appear to be disconnected as well with the thermal pad, contrary to the note on page 22 of the datasheet. The only pins that result internally connected are respectively 3, 4 and 8, 9.

Is this a possible isolated case on a certain batch? Please help us check and verify.

Thanks in advance!


Kind Regards,

Jejomar