Other Parts Discussed in Thread: SN6505B, SN6505A,
Hi
My customer wants to confirm whether the output can be 0.5A
Or suggest a suitable product
Input 5V to Output 5 V
Current 0.5A
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gareth,
For integrated transformer, control and switches, UCC12050 is the lowest profile, highest integration, lowest EM emissions, DC/DC bias converter module in its class but it is limited to 500mW, so 5V at 100mA is the output limit here. Another popular 5-V isolated bias option is SN6505A and SN6505B which is an open loop push-pull driver with integrated switches like UCC12050 but uses an external transformer and rectifying diodes. The external transformer enables SN6505x to easily handle up to 1A for a 5V bias output. Thanks for connecting through E2E.
Regards,
Steve M