This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
Hello Wang,
I have attached the file. The Current is stable with respect to line regulation (5V to 7V), but it's just not accurate ~20%. The Switching noise I can understand (although it's not good) .. it is what is happening in between the noise that I don't.
Thank you,
John
It could still be a switching noise. Please check the LODRV signal to see if it has transient in between HIDRV signal transience.
The bq24610 has a cycle-by-cycle UCP comparator to prevent the inductor current flowing back to input. So, if the inductor current is lower than the UCP threshold, the LODRV turns off the low side buck FET.