Other Parts Discussed in Thread: TPS53622
We use the TPS53622 regulator in our design for providing 2 phase power using only channel A in our design and we are seeing manufacturing failures. A query of the Status registers points us to the STATUS_MFR_SPECIFIC register. In this register the TSNS_LOW bit is set. The spec says this is due to "Latched flag indicating that TSEN ≥ 150mV before soft-start". The net is tied to your CSD95496QVM power stages. I need some better insight as to what might be causing this failure. Also, is there a way to tell if this is due to one specific CSD95496QVM or if it is the TPS53622? Any help here is much appreciated.
Data Points I see:
Spec says there are 3 ways TAO can be triggered to hold be a logic 0.
(1) The TSEN/TAO net must be below 150mV at soft turn on or else you get TAO held low. I see 160mV in the failed state. How do I tell which chip is holding this net low?
(2) The LSET resistor tied to GND must be a resistance less than 2Mohms. We use 110K
(3) If REFIN is detected to be above its maximum operating value. I see 1.7V which is the nominal voltage so I don't think this is the issue.
We see a roughly 2 % fallout for this issue in production.
Can the TPS53622 be the source of the TSEN/TAO net being low? How do you tell? Any ideas as to what could be causing this?
Thanks, Jim