Other Parts Discussed in Thread: UCC28180
Hi
Can UCC28065 use in a DC-DC 600W and the input 12~60Vdc application? Or there have other suggestions? thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Poster,
yes, UCC28065 can support DC input application.Since the input voltage is low, the peak current of mosfet still is high, you may need to add external driving IC for the mosfet.
UCC28180 which is single phase CCM controller also can support DC input. You can also consider it.