Other Parts Discussed in Thread: LM5164, LMR36506
Hi Sir,
Please confirm if lmr50410-q1 could pass Test B pulse without TVS protection?
1.customer’s requirement
2.ISO 16750-2:2012
Thanks,Ian.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
Please confirm if lmr50410-q1 could pass Test B pulse without TVS protection?
1.customer’s requirement
2.ISO 16750-2:2012
Thanks,Ian.
Hello Ian, for nominal 24V application and 59V load dump, often customer select 60V device say.
ABSMAX specification is usually interpreted as DC voltage unless otherwise specified.
LMR36506 or LM5164 might be good option.
Also have some options that are soon to be released publicly. You will need to contact me by email for those though.