Other Parts Discussed in Thread: TINA-TI, , TPS61288
Hi Team,
Per customer request, I need to run simulation to see transient performance. I tried to use Webench but it cannot export the transient model and cannot update to customer's condition. So please kindly help share me the transient simulation circuit using Tina-TI or please kindly help simulate on below condition. Thanks.
operation condition: Vin=3V, Vout=7V, Cout=44uf or 66uf.
load condition: change between 0 - 3.5A, rising time 1ns, falling time 1ns, period of 3.5A is 4us, one cycle time is 12us.
customer want to see the Vout overshoot/undershoot regarding the load transient. Thanks.
BRs
Given