This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP87561-Q1: Looking for a 1mV ripple solution, for 3.3V to 0.94V / 10A

Part Number: LP87561-Q1

Hi Expert

I am looking for 1mV output ripple solution, for 3.3V to 0.94V / 10A.

LP875761 looks good, but its Vout is fixed at 1V.

LP87561 seems to be the closest one, but still it needs more optimization on L/C to try.

Do you have some recommendations? 

Thanks!

-Rocky