Other Parts Discussed in Thread: LM5146-Q1
Hi,
My customer designs DCDC with LM5164-Q1. However, after staring FANs, LM5164-Q1 stopped SW output for 1 - 2 seconds. WHY does this phenomena occur? Please let us know how to resolve this.
Spec is as follows.
Input : DC 73V
Output : 12V
Load : DC FAN x 2
Phenomena:
- power-up and output 12V on LM5146-Q1.
- Start DC FANs
- After 1-2 seconds, SW output is stopped and decrease output voltage.
- After 1-2 seconds, LM5146-Q1 re-starts SW output and output is returned (12V).
- Then LM5146-Q1 keep working correctly.
Schematics is as follows:
Thanks and best regards,
M.HATTORI.