Other Parts Discussed in Thread: UCC2806, UC2846, UC3846
Planning to use the device in 50% duty-cycle, with a setup shown in the attached pdf.
NI,INV pins are set for 50% duty.
Considering pulling CURLIM and COMP pins to VREF via resistor to disable current limit.
[Questions]
[1]
Is the setup shown in the attached file acceptable for holding 50% duty while disabling current limit?
[2]
Not sure how the Transistor between Error Amplifier (EA) and CURLIM works...?
When EA output is MAX, does the transistor turn on, and current limit operation happens...?