Hi team,
I have one question about the current limit function.
current limit=100A
fast trip current=150A
Tflt=100ms
In normal operation, which means that Vin=Vo=12V, if the load wants 130A, can the power supply provide 130A to the load? Or the MOS will regulate the current to 100A?
In other words, I know that current limit function will regulate current <100A in start-up process. But I don't know if it's the same case in normal operation.
Thanks a lot!
Nison