Hi, TI expert.
I have a question about Min voltage (-voltage) of HS pin of UCC27712.
If you look at the datasheet, the Min voltage of HS pin is -11V in operating condition.
Q1) However, when measuring the HS pin during normal operation, Min (-11.3V) was measured. (Refer to Waveform-1)
In normal operation, HS-HB: 14.63V is measured as 15V under, but it is out of -11V, the Min spec of HB pin.
Is there any problem with the operation?
Q2) Also, if HS pin is measured during Peak Load operation, Min (-14.3V) is measured. (Refer to Waveform-2)
The HS-HB voltage is also 19.69V. Is there a problem with the operation?
[Waveform-1, HS pin Min voltage during Normal operation : -11.3V (CH1 : HS pin , CH2 : HS-HB , CH3 : Output current) ]
[ Waveform-2, HS pin Min voltage during peak load operation : -14.3V (CH1 : HS pin , CH2 : HS-HB , CH3 : Output current) ]
In the basic state of the scope without measuring any terminal, -2.5V is output. (Refer to Waveform-3)
[ Waveform-3, In the basic state of the scope without measuring any terminal ]
Please check.
Thank you.