This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I used LM63615-Q1 in my design at 5VDC output, the input voltage was 12VDC and the max load current drawn was 100mA. But unfortunately I had to see multiple failures almost 5 times out of 6.
Please suggest a reason/root cause analysis for this.
Regards
Avinav
Hi Avinav,
Can you upload the circuit and PCB layout design of LM63615 section?