Other Parts Discussed in Thread: , TPS65131
Hi,
I purchased the TPS65130 evaluation board (TPS65130EVM-839) for testing. The end application will be generating +/-12V rails from a 3.3V supply, with an expected load of ~50mA.
I modified the evaluation board feedback resistors to adjust the output voltages, but the negative rail is not working correctly. The positive rail is steady at 11.93V, as expected, but the negative rail is stuck around -0.1V.
The following components were changed:
- R4: 162kΩ → 100kΩ.
 - R2: 162kΩ → 100kΩ.
 - R5: 665kΩ → 1MΩ.
 
These changes should set the outputs to +/-12V according to the calculations in the applications section of the datasheet.
The voltage at the FBN pin is measuring -0.02V, and the voltage at the VREF pin is measuring 1.213V, both of which make sense. The layout can't be the issue with an eval board, and no other components have changed - has anyone resolved similar issues with this device?