Other Parts Discussed in Thread: BQ20Z80
Good afternoon,
I search to perform a "Golden Pack" with a BQ20z80_V110. I follow the procedure in SLUA3255B.
My problem concerns the phase 10 for "2 - Creating Pre-Learned Defaults" : "Reprogram the pack with a fresh .srec or .senc to clear all hidden constants".
Where can I find the file SENC for to integrate with tab PRO ? (I use BQ Evalation Sofware)
Another point :
Once I reprogram the Data Flash with the modified file (UpdateStatus=2 and Cycle count=0) the Max error registe returns to 148%.
How do I get a golden pack with Max Error = 1% (like the cycle learning) and UpdateStatus=2 and Cycle count=0.
The program BQ Evalation Sofware also generates a Golden Pack file with UpdateStatus=2 and Cycle count=0 but with a Max Error to 144% It's normal ??
Thank you in advance for the help.