Dear Sir/Madam,
I am planning to use the LM5116 in an application that has the following parameters.
Input : +48V
Output : +12V@8A.
I don't have any experience with this part so some advice would be much appreciated.
The schematic based on the web bench design is shown:
Q1. Are there any issues with using this controller to produce +12V @ 8A from a +48V input?
Q2. I plan to test using the +12V EVM part number LM5116-12EVAL/NOPB to test. With some minor component
changes is it possible to get 8A from the EVM?
Regards Grant