This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV61225

Other Parts Discussed in Thread: TLV61225

Hi!

I was wondering if the TLV61225 can be operated in shutdown mode with VIN 0V or VIN > 0V while VOUT is supplied from another source and > 0V. The datasheet mentions this:

During shutdown, the
converter stops switching and all internal control circuitry is turned off. In this case, the input voltage is connected
to the output through the back-gate diode of the rectifying MOSFET.

Does this mean, that current from the output to the input is blocked by the internal diode?

Thanks,

Peter