Other Parts Discussed in Thread: TL431, ATL431, , UCC28740
Dear Team,
My customer's output is unstable depending on the load current.
When the output voltage drop, the TL431 also not maintain at 2.5V.
Originally I thought is because of competitor's TL431 sink too much current.
So I suggest them to use ATL431, but the issue is the same.
Do you think smaller PR62 will help here?
I am worried if smaller PR62 solve the customer the issue, they will still use competitor's TL431.
Do you have any suggestion on it?
BR
Kevin