Part Number: BQ24295
Hi
This is the schematic of BA24295 in my board:
I don't change its registers and use its default setting.
when the USB charger is plugged in, the output is 4.8 volts. after removing it I see a 2-volt drop on PMID for about 50 ms and then It comes up to the 5.1 volts.
Is this drop voltage normal? How can I prevent it?