Other Parts Discussed in Thread: EV2400, BQSTUDIO
Hello
I succeded to use the bq40z50EVM with the EV2400 and bqtudio. I'm simulating a battery pack 3Swith an external power (3.7 x 3 = 11.1V) an 3 x 1K resistors as suggested in the manual.
In these conditions, after powering the EVM and pressing the Wake button the device is properly recognized. In the same conditions but with a 10 Ohm load connected between PACK+ and PACK-
the device is not recognized!!! But if I start with no load and after BQstudio has recognize the device I attach the laod everithing works fine. (for example issueing a DSG_FET_TOGGLE command I see about
1A flowing through the load).
I don't undertand why the device is not recognized in presence of a load when I power up the EVM. A possible reason is that the device in in SHUTDOWN but why?
Any help?
Thank