This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 65
Part Number: TPS61099
Hi Sir,
My customer using TPS61099 and fund 3pcs( of 200pcs) FB over spec. cause Boost voltage is a little bit HIGH.
Pls double check if below FB is make sense? How about the range?
Thanks, Ian.
Hi Ian:
What's the load condition during the test?
If the converter operate in PFM, it's normal. As the spec in datasheet just for typical value.And generally, PFM has a little larger ripple than PWM mode.
Best Regards
Minqiu
In reply to Minqiu Xie:
Hi Guys,
A: no laod&at PFM mode
If the converter operate in PFM, it's normal.
A: so that will be 1.031~1.039V ?? or ?
In reply to Ian Wang:
If it's operating in burst mode, the ripple will larger than normal. And if you measure the Vout (same as FB pin), you will find the different from PWM mode. (Like figure 19 in datasheet)
And we don't guarantee an exact spec for its range.