Hi experts,
My customer have 3 circuits that use the TPS7A8300. Each has a VIN of 1.2V, 1.4V, and 1.8V. The BIAS to all of them were connected to 5V. Can they leave the 5V connected to BIAS when VIN is 1.4V and 1.8V, or do they need to disconnect the 5V from the BIAS pin?
Any disadvantages for leaving the BIAS connected to 5V?
Thanks,
Connie