Hi,
I am building a sample environment for PROFINET at "PRU-ICSS-Profinet_Slave_01.00.03.04" (IRT).
The environment is as follows:
・PRU-ICSS-Profinet_Slave_01.00.03.04
・processor_sdk_rtos_am57xx_5_01_00_11
・ccs_8.1.0.00011
・XDC_TOOLS_VERSION=3.50.07.20
・SYS_BIOS_VERSION=6.73.00.12
・NDK_VERSION=3.40.01.01
・EDMA_VERSION=2.12.05.30
We are developing am572x PROFINET IRT(LAN 1PORT) based on this sample.
Each stack is the same as the sample.
Two LAN PORTs are supported in the sample. (PORT1 / PORT2)
The HW we are developing uses only this PORT2 side to make it a 1PORT PROFINET product.
Therefore, I would like to treat the data communication with the PORT2 side of the sample environment as the data communication with the PORT1.
A block diagram is attached.
By exchanging Linkup informPORT replacement question AM572x .xlsxation etc. between PORT1 and PORT2, "RT" communication has become possible.
But, "IRT" communication is not possible.
Q1. Is IRT communication feasible under the above conditions (replacement of LAN PORT1 and LAN PORT2)?
Q2. (Q1 If yes,) Where should I change?
Thank you for your confirmation.
Best regards,
Eiji