Other Parts Discussed in Thread: AM5718
Hi Ti
How to modify PRU MII power from 3.3 to 1.8V?
Which power Pins control MII power?
Same as RGMII(vddshv9 W4/ W5/ U10) or not ?
Foxcomn
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ti
How to modify PRU MII power from 3.3 to 1.8V?
Which power Pins control MII power?
Same as RGMII(vddshv9 W4/ W5/ U10) or not ?
Foxcomn
Seem RGMII can not work by 2.5V? Just 1.8V and 3.3V.
Is same as PRU MII?
The TMDXIDK5718 EVM only supports 3.3V IO for the PRU MII. However - the processor (AM5718) supports either 1.8V or 3.3V on all of its LVCMOS IO, including those IO that support PRU MII. The AM5718 devices does not support 2.5V IO.
I can not find the MII Power Pin definition in the datasheet?
Do you know which one?
In the data manual, Table 4-2 (ball characteristics) list each ball, and the various functions supported on those pins. The power column defines which IO power rails that pins is supported. (Each ball support multiple functions, some including MII functions).
Also - IOSETs for PRU-ICSS MII interfaces are listed in Table 7-154, 155, and shows the associated ball location.