Team,
Where should the GPIO_4 (PMIC_WAKE1) of PMIC-1(TPS65941213-Q1) to be connected. I could not able to fetch the same from the PDN. Similarly for PMIC-B - GPIO 10 (PMIC_WAKE2).
Thanks
arun
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
Where should the GPIO_4 (PMIC_WAKE1) of PMIC-1(TPS65941213-Q1) to be connected. I could not able to fetch the same from the PDN. Similarly for PMIC-B - GPIO 10 (PMIC_WAKE2).
Thanks
arun
GPIO_4/PMIC_WAKE1 is an used as an external wake input. For example, if system in a low power mode (like Suspend to RAM), signal could be used to wake the system up and back to active mode. GPIO-10/PMIC_WAKE2 is similar function.
If We are not using the option, can we pull the particular GPIO pin down or is it required to specify some state ?
Yes - these pins do not force INTO a low-power state, but used to WAKE from low-power state. If unused, the pins can be pulled low.