This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: AM64x power supply and compatibility

Part Number: AM6442
Other Parts Discussed in Thread: AM6421

Hello, I have questions about AM64x.

Question 1:
AM64x VDD_CORE can be selected from 0.75 or 0.85V. Is this determined by the model number? Could you tell me the difference between them?

Question 2:
VDDS_DDR can be selected from 1.1 or 1.2V. Is this determined by the DDR used?
DDR4:1.2V
LPDDR4:1.1V

Question 3:
Is it possible to replace the AM64x series without change because it is pin compatible?
My customers designing with AM6442 are considering  and replace it with AM6421.

Regards,
Rei

  • No, all devices will operation with either 0.75 or 0.85V VDD_CORE.  There are several other voltage rails which require 0.85V, so you can either combine all those rails for a simplified power solution, or you can implement VDD_CORE=0.75 to reduce power consumption

    Yes, DDR type will determine the DDR IO voltage VDDS_DDR

    Yes, these device variants are pin compatible

    Regards,

    James

  • Thank you very much!