This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We see a problem with simultaneous operation of EMIFA in Extended Wait Async mode and EDMA3 SPI.
CPU reads data via EMIFA with EM_WAIT control. EDMA3 reads and writes data via SPI.
Both interfaces demonstrate no errors if run separately.
If the interfaces operate in parallel and EM_WAIT lasts more than period between EDMA3 SPI events, we observe a loss of EDMA3 SPI words and EDMA3 detects missed events.
For debugging we detach EM_WAIT from external memory and control memory stall with AWCCR.MAX_EXT_WAIT. We observe the same losses at different SPI speeds.
Where is the conflict? May EDMA3 transfer data during CPU memory stall?
Best regards,
Irina
Hi James,
EMIFA interface was tested without external memory - memory stall was set with AWCCR.MAX_EXT_WAIT. EDMA3 SPI and EDMA3 UART were tested with various devices, including a personal computer using a factory-built converter. Losses were the same in all cases of simultaneous operation.
All interfaces use L2 RAM space: CPU reads data via EMIFA to the registers and writes data to L2 RAM buffer
in the next instruction, EDMA3 SPI reads and writes data to other L2 RAM buffers.
Is such use of L2 RAM space critical?
We tried to use L1D RAM as destination buffer for EMIFA, but the behaviour was the same - errors.
Best regards,
Irina
Irina, i don't think the memory that you are using is the issue. In the first post, you said that EDMA is reporting missed events. What is triggering each EDMA event? Does it have anything to do with the EMIFA transactions?
Regards,
james
Hi James,
EDMA3 SPI events - SPIREVT and SPIXEVT - arise when a character is received and when a character is to be transmitted via SPI. These events are not related with the EMIFA transactions.
Best regards,
Irina
Irina, it seems like the same SCR (switched cental resource) is controlling both transactions, and when it has to wait for a long time because of the EM_WAIT, it is preventing other masters from accessing that memory
You may have to adjust the master priority in the system. See section 10.3 of the TRM for more details. Ensure the EDMA module you are using has higher priority than the CPU.
Regards,
James
Hi James,
DSP MDMA default priority is 2. EDMA3_0_TC1 which is used for SPI default priority is 0 (highest). So EDMA module priority is higher than the CPU.
We set 7 (lowest) DSP MDMA priority via MSTPRI0. The behaviour was the same - errors.
Best regards,
Irina
Irina, since you are accessing the L2 RAM space, i believe you have to configure the Bandwidth Manager (BWM) inside the DSP subsystem, since that has control over those memories. See section 2.2.2.3 of the TRM. SPRUFK5 is the doc for the DSP Megamodule Reference Guide, which will have the details of this DSP peripheral.
I think what you are trying to do is possible, we just have to figure out how to configure the internal paths to enable and prioritize it correctly
Regards,
james
Hi James,
CPU default priority for L2 access is 1 (CPUARBU register). SDMA priority for L2 access is dictated by the external system master transfer parameters, EDMA3_0_TC1 default priority is 0 (highest). So EDMA module priority for L2 access is higher than the CPU.
We set CPU L2 priority 6 via CPUARBU. The behaviour was the same - errors.
Errata (sprz304h) says "Advisory 2.3.1 - DMA Access to L2 RAM Can Stall When DMA and C674x CPU Command Priorities Are Equal", but default priorities aren't equal.
Best regards,
Irina
Irina, i think the distinction here is that the priority arbitration only comes into play for pending requests. In your case, the EMIF request has already been granted and is in progress, and BWM is waiting for the for it to finish while the EDMA request arrives. Thus it would have to abort the EMIF transaction (or somehow pause it) to let the EDMA transaction complete to the L2 RAM. I don't think this is happening.
Just as an experiment, do you have another memory in your system to work with, just to see if the bottleneck is the L2 RAM? I'm not suggesting this as a solution yet, just want to confirm the final operation is functional.
There is a small memory in the PRUSS that you might be able to use for this purpose.
Another idea is to reduce the MAXWAIT parameter as mentioned in the errata note. This may allow the EDMA transaction to complete.
Regards,
james