This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have noticed that the AMIC110ICE_EVM board for the DDR3 interface no termination resistors (address & control lines) are provided. Accordingly a corresponding VTT control is also missing.
With the AM335X EVM board both (as usual) is present.
My questions:
- Can I take over the DDR3 circuitry from the AMIC110_EVM without problems, even if I don't use the same DDR3 chip (MT41K256M16TW)?
- What are the reasons that caused TI to deviate from the "standard" circuitry?
Regards Bernd
Bernd, a "no VTT" topology is allowed if you only have one DDR device so all signals are point-to-point connections. The AM335x EVM has a fly-by topology with multiple devices, necessitating the need for VTT. Note that some devices have multiple dies in one package, and this would also require VTT. Only single device, point-to-point signaling would be allowed with no VTT
Regards,
James