hi,
can you please point the place in the DM814x data sheet that mention the value of the end termination resistors for the addresses, controls and clocks?
i can't find it there. the data sheet only reffer to it as Zo. i can see a value if using DDR2 but not for DDR3 design.
in my design i use the configuration shown in Figure 8-55. 32-Bit, One-Bank DDR3 Interface Schematic Using Four 8-Bit DDR3 Devices.
It's taken from page 305 in the data sheet - SPRS647E –MARCH 2011–REVISED DECEMBER 2013
thanks.