Hello,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Sorry, I have read the post Can't boot C6A8168 EVM board from SD card (http://e2e.ti.com/support/dsp/integra_dsparm/f/625/t/86416.aspx) and I have found the file mksdboot.sh. So now, I have understood how to create a boot SD card. But I am still wondering if it is possible to boot from NAND without the XDS560 emulator.
JS
Hi Jean,
you can boot from NAND without an emulator/debugger; you need to flash the NAND using Uboot itself. See my post for details:
http://e2e.ti.com/support/dsp/integra_dsparm/f/625/t/100154.aspx
By the way, please let me know if you get it working as I didn't and it would be good to know if someone else did!
Thanks,
Ralph
Hi,
There is something I definitively do not understand. At which moment do I am supposed to enter commands to be executed on the target ? At no time I can see this line where I could enter something :
TI8168_EVM#
Is it accessible from minicom ? I do not manage to make minicom work. And without it, i presume that I can't configure the NAND or anything else. And yet, at each tilme, I tried to follow the steps. For instance, after having executed the file setup.sh in the folder ti-ezsdk_c6a816x-evm_xx_xx_xx_xx : I do all the steps by keeping the standard parameters and at the end, I am asked :
"Would you like to run the setup script now (y/n)? This requires you to connect"
"the RS-232 cable between your host and EVM as well as your ethernet cable as"
"described in the Quick Start Guide. Once answering 'y' on the prompt below"
"you will have $timeout seconds to connect the board and power cycle it"
"before the setup times out"
"After successfully executing this script, your EVM will be set up. You will be "
"able to connect to it by executing 'minicom -w' or if you prefer a windows host"
"you can set up Tera Term as explained in the Software Developer's Guide."
"If you connect minicom or Tera Term and power cycle the board Linux will boot."
I connect the cables, I press y, minicom is started (but stops at "Press CTRL-A Z for help on special keys"), I connect the EVM, my computer (host) detects an ethernet connection during 30 seconds (or so) then it stops, and nothing more. I think it must be because I have not plugged the SD card, but I am not sure. There is probably something I have not understood in the different steps of booting (I am new in developping such applications...). Anyway, fas I have explained in my precedent post, I have no SD card for the moment. Is it really impossible to work without it ?
I thought that booting on NAND, NOR or SPI were some alternatives for people who do not want to use the SD card.
Thanks.
JS
Where is downloadering the EZSDK for the C6A8168 EVM ??
Can you support the address where can downloader the right EZSDK for the C6A8168 EVM????
Thanks!!