Is the J721EXCPXEVM support 8M pixel video input via VPFE ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As, it can support 8MP resolution, but pixel clock will be limited to 100MHz, so fps will be limited.
But please note that VPFE is not supported yet in the SDK.
Hello
but what else function to supoort the 8M pixel if we compromise FPS rate as of now?
Sorry, did not get your question. Do you mean what else is supported or needs to be added for 8M sensor?
one more question, which 8M image sensor has already supported in TI? We would like to know the type of image sensor that has supported by TI -SDK .
SDK supports AR820 sensor, which can output 8MP resolution.
Regards,
Brijesh