Hello,
i m trying to run Hello World project on beaglebone black based on am3358 sitara processor. I have following configuration:
- beagle bone black
- spectrum digital XDS100v2 debug probe
i manually soldered wires on 20 pin jtag pads on beaglebone board to a 14 pin strip, that i use to connect to the emulator.
onto CCS (v10.4) i have created an "hello world" project with target configuration file, and successfully passed the "test connection".
When i launch debug on CCS, it can t connect to the target (cortexA8 processor), and gives the following error:
why i get this error and how i can get rid of it?
is my xds100v2 probe with 14pin JTAG connector compatible with AM3358 on BB black?
please give hints, thank you
Kind Regards
Emanuele Peruzzi