Environment:
- Board: TMDS243GPEVM (bought from TI website)
- Debugger: onboard XDS110 with microAB USB connector
- IDE: CCS 10.3.1
- SDK: AM243X/08_01_00_25, AM243X/08_01_00_14, AM243X/08_00_00_21
Use case:
I use AM243X/08_01_00_25 to flash SOC initialization binary to the new board for the first time follow https://software-dl.ti.com/mcu-plus-sdk/esd/AM243X/08_01_00_25/exports/docs/api_guide_am243x/EVM_SETUP_PAGE.html#EVM_FLASH_SOC_INIT,
all commands executed successful. Change boot mode from UART boot mode to OSPI boot mode, then power on, the information shows in UART terminal is correct.
But when I try to connect to core_R5_0_0, CCS popup an error window, see below picture.
I try to use AM243X/08_01_00_14, AM243X/08_00_00_21 to check, but get the same error result.
I try to download DMSC firmware directly by using script in NOBOOT mode, but get the same error result.
I don't know how to resolve this problem.