Hi,
The customer has a question about the MMCSD driver below.
In the MMCSD_v1.c, SDVS [bit 11:9] in the MMCHS_HCTL register is started from setting 0x6 (3.0V), but it’s started from 0x7 (3.3V) in the MMCSD_v2.c.
What does this difference impact ? What does this change mean ?
Used SD card : UHS support SD card (Speed class I)
Device : AM5746
Dev Environment : CCS v8
Compiler : GCC GNU v6.3.1 (Linaro)
Hardware : AM5746 customer’s own board
Software : pdk_am57xx_1_0_11
OS : Bios_6_76_00_08
XDCTools : 3.50.3.33
ICE : Lauterbach
Regards,
Hideaki