This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: TDA4 PCIe issue

Part Number: TDA4VM

Hi~

    1. How can I get or set the PCIe Preset values on TDA4 after linking up?

    2. Does TDA4 support digital eye diagram?

    3. Is the Preset values obtained by the PCIe auto-negotiation mechanism the optimal solution?

 

  • Billy, 

    There are no documented registers/structure to read presets. I assume you want to perform compliance testing, to do so:

    You can use the EC bit in the RC to force the EP to enter compliance mode, the EC bit is the  PCIE_CORE_RP_I_LINK_CTRL_STATUS_2[4] register bit. you can use devmem2 utility to set the register directly. 

    regards

    Jian